This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430 SD-16A



When SD-16A in unipolar input mode and the common mode voltage is zero,  Can be measured accurately at the level of mV DC voltage?
In other words, a pair of differential input to the ground, SD-16A conversion results in theory can be achieved, can it be used?
We need to deal with the models are relative to the  level mV DC small signal

  • Alvin,
    If I'm understanding correctly, yes you should be able to take measurements in the mV range. Your measurement step size will depend on your reference voltage, given as VREF/2^16. Which is 18uV for a 1.2V Reference.

    If you have further questions, can you please tell me which MSP you are using?

**Attention** This is a public forum