Part Number: MSP430FR2633
In the datasheet it lists two values, a max and a min for the Vinput threshold. In this case at VCC = 3V then Vit (min) =1.35V and Vit (max) = 2.25V. I assume this means the worst case Vit across any part that I might buy would be 2.25V correct? Or is that max number a do not exceed number, as in do not drive more than 2.25V into any input?
Thank you