This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP430F5659: MSP430F5659 RAM issue

Part Number: MSP430F5659

Tool/software: Code Composer Studio

Hello all,

A customer ask:

I am using the MSP430F5659 and I have an application which needs RAM more than 16 KB. It should not be a problem, because the MSP430F5659 has 64KB RAM. However now I see in the "Memory Allocation" - Windows of Code Composer two RAMs: RAM and RAM2 ?
RAM has a size of 16384 Byte
RAM2 has a size of 49152 Byte
????
As soon the code needs more than 16KB, lots of warnings are coming: something like "pointer to long" for 16 Bit or so. What is this?
I thought, that the MSP430F5659 has a RAM with really 64KB?

Could anyone help me this question.

Thank you in advance.

Kaustubh

**Attention** This is a public forum