Part Number: MSP430FR2311
Other Parts Discussed in Thread: CC1200
Hi,
(This is my first attempt on MSP430) I am now porting custom BSL from slaa600 to MSP430FR2311 using IAR 6.5. I am done with the BSL but in APP2, I have issue while try to mapping the "real" interrupt table(0xFF80~0xFFFF) to proxy interrupt table. I already search some threads about custom BSL but not much information.
In the G model I found the mapping can be done like this
extern __interrupt void P1_Isr(void);
extern __interrupt void Dummy_Isr (void);
# ifdef __IAR_SYSTEMS_ICC__
# pragma location="APP_PROXY_VECTORS"
__root const uint16_t ProxyVectorTable[] =
# elif defined (__TI_COMPILER_VERSION__)
# pragma DATA_SECTION(ProxyVectorTable, ".APP_PROXY_VECTORS")
# pragma RETAIN(ProxyVectorTable)
const uint16_t ProxyVectorTable[] =
# endif
{
0x4030, (uint16_t) P1_Isr, // APP_PROXY_VECTOR(0) P1
0x4030, (uint16_t) Dummy_Isr, // APP_PROXY_VECTOR(1) P2
0x4030, (uint16_t) Dummy_Isr, // APP_PROXY_VECTOR(2) ADC10
0x4030, (uint16_t) Dummy_Isr, // APP_PROXY_VECTOR(3) USCI SPI TX
0x4030, (uint16_t) Dummy_Isr, // APP_PROXY_VECTOR(4) USCI SPI RX
0x4030, (uint16_t) Dummy_Isr, // APP_PROXY_VECTOR(5) TA0_1
0x4030, (uint16_t) Dummy_Isr, // APP_PROXY_VECTOR(6) T0_0
0x4030, (uint16_t) Dummy_Isr, // APP_PROXY_VECTOR(7) WDT
0x4030, (uint16_t) Dummy_Isr, // APP_PROXY_VECTOR(8) COMP_A
0x4030, (uint16_t) Dummy_Isr, // APP_PROXY_VECTOR(9) TA1_1
0x4030, (uint16_t) Dummy_Isr, // APP_PROXY_VECTOR(10) TA1_0
0x4030, (uint16_t) Dummy_Isr, // APP_PROXY_VECTOR(11) NMI
0x4030, (uint16_t) Dummy_Isr,
0x4030, (uint16_t) Dummy_Isr,
0x4030, (uint16_t) Dummy_Isr,
};
But, in the FR model, it shows
// // Constant tables // /* Proxy table is not needed for FR5xx */
Question 1: why there is difference in G model and FR model, if there is no code available in FR model, so how proxy vector table is mapped to interrupt table?
I try to copy the G model to FR to make it work (like above), but failed. And show a lot of errors
Error[Pa128]: truncating cast in constant expression...
# ifdef __IAR_SYSTEMS_ICC__
# pragma location="APP_PROXY_VECTORS"
__root const uint32_t ProxyVectorTable[] =
# elif defined (__TI_COMPILER_VERSION__)
# pragma DATA_SECTION(ProxyVectorTable, ".APP_PROXY_VECTORS")
# pragma RETAIN(ProxyVectorTable)
const uint32_t ProxyVectorTable[] =
# endif
{
0x4030, (uint32_t) P1_Isr, // APP_PROXY_VECTOR(0) P1
...
I change from uint16_t to uint32_t, the error gone, but it does not jump to the interrupt function when button at port 1 is pressed, it shows there is something happen when I press the button by stop at address 0x10000 which is out of memory size (the maximum is 0xFFFF for FR2311). Therefore, I think the mapping is wrong so the it cannot jump to the correct vector.
Question 2: why with the G model the uint16_t can be used but show error in FR2311? And since I need to change it to uint32_t, my proxy interrupt table becomes very big which wasting FRAM (FR2311 only has 3.75kB FRAM)
As I see in the memory map, the actual interrupt vector table from 0xFF88~0xFFFF, meaning there is 120 bytes, but most of them are unused, only 15 interrupt vectors are defined in msp430fr2311.h
#define ECOMP0_VECTOR (45 * 2u) /* 0xFFE2 */ #define PORT2_VECTOR (46 * 2u) /* 0xFFE4 */ #define PORT1_VECTOR (47 * 2u) /* 0xFFE6 */ #define ADC_VECTOR (48 * 2u) /* 0xFFE8 */ #define EUSCI_B0_VECTOR (49 * 2u) /* 0xFFEA */ #define EUSCI_A0_VECTOR (50 * 2u) /* 0xFFEC */ #define WDT_VECTOR (51 * 2u) /* 0xFFEE */ #define RTC_VECTOR (52 * 2u) /* 0xFFF0 */ #define TIMER1_B1_VECTOR (53 * 2u) /* 0xFFF2 */ #define TIMER1_B0_VECTOR (54 * 2u) /* 0xFFF4 */ #define TIMER0_B1_VECTOR (55 * 2u) /* 0xFFF6 */ #define TIMER0_B0_VECTOR (56 * 2u) /* 0xFFF8 */ #define UNMI_VECTOR (57 * 2u) /* 0xFFFA */ #define SYSNMI_VECTOR (58 * 2u) /* 0xFFFC */ #define RESET_VECTOR (59 * 2u) /* 0xFFFE */
here is my linker file of APP2:
// Application Checksum address -D_Appl_Checksum=_FLASH_START -D_Appl_Checksum_8=(_FLASH_START+2) // Application Start address (after checksum) -D_Appl_Start=(_FLASH_START+3) //F100+3=F103 // Application End Address -D_Appl_End=(_BOOT_Start-1) //F388-1=F387 // Application reset vector -D_Appl_Reset_Vector=(_Appl_End-1) // Start address of Proxy vector table -D_Appl_Proxy_Vector_Start=(_Appl_Reset_Vector-30) // End address of Proxy vector table -D_App_Proxy_Vector_End=(_Appl_Reset_Vector-1) // Size of area calculated by CRC (App+ProxyTable) -D_CRC_Size=(_Appl_End-_Appl_Start+1) -Z(CONST)APP_PROXY_VECTORS=_Appl_Proxy_Vector_Start-_App_Proxy_Vector_End -Z(CODE)INTVEC=_Appl_Proxy_Vector_Start-_Appl_End -Z(CODE)RESET=_Appl_Reset_Vector-_Appl_End
Question 3: So, can I only use 30 bytes in the the proxy vector table in my app to save memory? If not, please suggest what size of the proxy vector table to use all above interrupts (in case I want to use it), and why?
Question 4:I see in the "Custom ISR structure", the file "interrupt proxy.asm" is added directly to IAR project, is it possible to add assembly .asm file like that?(the compiler understand? Or any configuration must be set? ). I try to add it and it seems the linker doesn't understand where to call #include "msp430fr2311.h"
Question 5: How to map proxy interrupt table to the real interrupt table in IAR?
thank you