Other Parts Discussed in Thread: MSP430WARE
Tool/software: Code Composer Studio
I was able to create a project in CCS7 for the MSP430F5510. I was able to manipulate I/O bits on my custom PCB.
I'm now trying to use driverlib.h in CCS7 for a new project based around the same MSP430F5510 based prototype. I used the new project wizard. However, there is no listing in the templates for MSP430Ware.
I then tried to import driverlib.h manually.
If I import all of the files in C:\ti\msp\MSP430Ware_3_60_00_10\driverlib\driverlib\MSP430F5xx_6xx to the project root directory, then the project builds fine, without errors. However, this really makes a mess of the project directory.
If I add a new directory called "driverlib" to my project and then import the files in the above directory to the "driverlib" directory, then the build fails, indicating the driverlib.h was not found.
How can I get the project to find driverlib.h if I put the files in a subdirectory?
Thank you for your help.