Part Number: MSP430F5308
Hello Team,
Can you help clarify the mapping capability for MSP430F5308? In particular, I see in table 1 of the datasheet that only the RGC and ZQE packages support 2xI2C channels, since port 3 pins are not included on the PT and RGZ packages, however I also see that USCI_B0 is listed in the mapping capabilities for port 4 in table 8. Is it possible to map both I2C modules to the P4 port? For example:
Pins 4.1/4.2 = USCI_B1 I2C port
Pins 4.6/4.7 = USCI_B0 I2C port
Best Regards,
Casey McCrea