Other Parts Discussed in Thread: MSP430F2274
Right now I got a litlle bit stuck on the following project:
I´m trying to control 3 motors at the same time with the msp430. The
speed will be regulated with PWM, and the input I will want to control
it with 3 potenciometers. One POT for each motor. The way that I´m
trying to do that is using de DTC to store 3 samples, one sample of
each POT and read it back using ADC10SA pointer. Each value of the POT
will be converted directly to the PWM duty cicle.
So, therre is something that will not work, when I hook it up I´ll see
a wierd square wave (I think in P2.3), with some strange duty cicle,
and it will romain constant even if we vary the POT's. And in the other
3 PIN´s that should give me some more PWM do not respond.
Could someone please tell me why?
Thank you so much in advance for all your time.
CODE:
#include "msp430x22x4.h"
unsigned int DATA[3];
void main(void){
WDTCTL = WDTPW + WDTHOLD; // Stop WDT
//ADC SETTINGS
ADC10CTL1 = INCH_2 + CONSEQ_1; // A2/A1/A0, single sequence
ADC10CTL0 = ADC10SHT_2 + MSC + ADC10ON + ADC10IE;
ADC10DTC1 = 0x03; //3 Conversions
ADC10AE0 |= 0x07; //Set A2 A1 and A0 as ADC10 inputs
//PWM SETTINGS
P2DIR |= 0x18; //Setting P2.3 and P2.4 as outputs
P2SEL |= 0x18; //Selecting the special function of P2.3 and P2.4 for the PWM
P4DIR |= 0x10; //Setting P4.4 as output
P4SEL |= 0x10; //Selecting the special function of P4.4 for the PWM
TACCR0 |= 1023; //setting duty period of TimerA
TBCCR0 |= 1023; //setting duty period of TimerB
TACCTL1 = OUTMOD_7;
TACCTL2 = OUTMOD_7;
TBCCTL1 = OUTMOD_7;
//Program initialitzation
for(;;){
//Sampling ADC10
ADC10CTL0 &= ~ENC;
while(ADC10CTL1 & BUSY); //Wait if the ADC10 core is active
ADC10SA = (unsigned short)&DATA;
ADC10CTL0 |= ENC + ADC10SC; // Sampling and conversion start
ADC10CTL0 &= ~ENC;
ADC10CTL0 = 0; // Power down the ADC
//Setting PWM
TACTL = TASSEL_2 + MC_1;
TACCR1 = DATA[3];
TACCR2 = DATA[2];
TBCTL = TBSSEL_2 + MC_1;
TBCCR1 = DATA[1];
}
}