Part Number: MSP430F67471
Other Parts Discussed in Thread: MSP430F147, MSP430F148, MSP430FG438
Hi champs,
cust is using the temperature sensor embedded in the MSP430F67471IPZR.
After a single-point calibration, as recommended in Note (4) of the datasheet, p. 91, we still see big discrepancies at other temperatures (slope problem). In our case, the single-point calibration was performed at +20 °C. Device brought to the temperature -40 °C, reads back only -30 °C. Theoretically one could perform a double-point calibration as described in chapter 1.13.5.3 of the User’s Guide (SLAU208O), however it is unpractical and extremely time consuming:
The User’s Guide presents a typical sensor transfer function as follows:
According to this function, the slope is TCsensor = 2.52 mV per °C.
Question:
how reproducible is this slope for different MSPs?
I find no specification of the TCsensor neither in the Datasheet nor in the User’s Guide (SLAU208O).
Can you provide me with the specification of the temperature sensor, please?