This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDM-WLMOTORMONITOR: TechBasic source code - Graphing FFT

Part Number: TIDM-WLMOTORMONITOR


Hi All,

I was wondering if anyone knows where is the ipad source code located for the TechBasic platform the design guide referring to. (tidu886.pdf, page 13, section 5.2.2) 

Regards,

Tibor

  • !Wireless Motor Monitoring CC2650 Radio Protocol
    !Edited by M. Raleigh
    !10/27/2014
    !Notes
    !
    !
    
    PRINT
    PRINT "This is a console program to rx/tx data from the WMMU via the CC2650 BLE Radio."
    PRINT
    PRINT "Press the Stop button to stop this program."
    PRINT
    connected = 0
    System.showConsole
    
    
    DIM zTemp AS INTEGER
    zTemp = 1
    
    DIM modecode AS INTEGER
    modecode = 93
    
    DIM firstvalue AS INTEGER
    firstvalue = 15000
    
    DIM RXData AS INTEGER
    RXData = 66
    
    
    DIM commandsAllowed AS INTEGER, commandTime AS DOUBLE, delay AS DOUBLE
    delay = .5
    
    ! Set up variables to hold the peripheral and the characteristics
    DIM WMMURadio AS BLEPeripheral
    
    
    
    ! Create the plots and arrays to hold the plot points.
    DIM p as Plot, px as PlotPoint
    DIM zDataBuff(400, 2)
    
    ! Create the controls.
    DIM quit AS Button, send AS Button, samples AS Button, fourier AS Button, nextKHz AS Button, nextKHz2 AS Button, nextKHz3 AS Button, nextKHz4 AS Button
    
    ! Create and initialize the global tracking variables.
    fileName$ = "wmmu_data.txt"
    
    !Init GUI
    !setUpGUI
    
    
    ! We will look for these services.
    DIM servicesHeader AS STRING, services(1) AS STRING
    servicesHeader = "-0451-4000-B000-000000000000"
    services(1) = "FFF0"
    accel% = 1
    
    ! Start the BLE service and begin scanning for devices.
    debug = 0
    BLE.startBLE
    DIM uuid(0) AS STRING
    BLE.startScan(uuid)
    
    
    ! Called when a peripheral is found. If it is a WMMU, we
    ! initiate a connection to it and stop scanning for peripherals.
    !
    ! Parameters:
    !    time - The time when the peripheral was discovered.
    !    peripheral - The peripheral that was discovered.
    !    services - List of services offered by the device.
    !    advertisements - Advertisements (information provided by the
    !        device without the need to read a service/characteristic)
    !    rssi - Received Signal Strength Indicator
    !
    SUB BLEDiscoveredPeripheral (time AS DOUBLE, _
                            peripheral AS BLEPeripheral, _
                            services() AS STRING, _
                            advertisements(,) AS STRING, _
                            rssi)
    IF peripheral.bleName = "SimpleBLEPeripheral" THEN
    WMMURadio = peripheral
    BLE.connect(WMMURadio)
    BLE.stopScan
    END IF
    IF peripheral.bleName = "Simple BLE Peripheral" THEN
    WMMURadio = peripheral
    BLE.connect(WMMURadio)
    BLE.stopScan
    END IF
    END SUB
    
    ! Called to report information about the connection status of the
    ! peripheral or to report that services have been discovered.
    !
    ! Parameters:
    !    time - The time when the information was received.
    !    peripheral - The peripheral.
    !    kind - The kind of call. One of
    !        1 - Connection completed
    !        2 - Connection failed
    !        3 - Connection lost
    !        4 - Services discovered
    !    message - For errors, a human-readable error message.
    !    err - If there was an error, the Apple error number. If there
    !        was no error, this value is 0.
    !
    SUB BLEPeripheralInfo (time AS DOUBLE, _
                      peripheral AS BLEPeripheral, _
                      kind AS INTEGER, _
                      message AS STRING, _
                      err AS LONG)
    IF kind = 1 THEN
    ! The connection was established. Look for available services.
    IF debug THEN PRINT "Connection made."
    peripheral.discoverServices(uuid)
    ELSE IF kind = 2 OR kind = 3 THEN
    IF debug THEN PRINT "Connection lost: "; kind
    BLE.connect(WMMURadio)
    ELSE IF kind = 4 THEN
    ! Services were found. If it is one of the ones we are interested
    ! in, begin discovery of its characteristics.
    DIM availableServices(1) AS BLEService
    availableServices = peripheral.services
    FOR s = 1 to UBOUND(services, 1)
    FOR a = 1 TO UBOUND(availableServices, 1)
    print availableServices(a).uuid
    IF services(s) = availableServices(a).uuid THEN
      IF debug THEN PRINT "Discovering characteristics for "; services(s)
      peripheral.discoverCharacteristics(uuid, availableServices(a))
    END IF
    NEXT
    NEXT
    END IF
    END SUB
    
    
    ! Called to report information about a characteristic or included
    ! services for a service. If it is one we are interested in, start
    ! handling it.
    !
    ! Parameters:
    !    time - The time when the information was received.
    !    peripheral - The peripheral.
    !    service - The service whose characteristic or included
    !        service was found.
    !    kind - The kind of call. One of
    !        1 - Characteristics found
    !        2 - Included services found
    !    message - For errors, a human-readable error message.
    !    err - If there was an error, the Apple error number. If there
    !        was no error, this value is 0.
    !
    SUB BLEServiceInfo (time AS DOUBLE, _
                  peripheral AS BLEPeripheral, _
                  service AS BLEService, _
                  kind AS INTEGER, _
                  message AS STRING, _
                  err AS LONG)
    IF kind = 1 THEN
    ! Get the characteristics.
    DIM characteristics(1) AS BLECharacteristic
    characteristics = service.characteristics
    FOR i = 1 TO UBOUND(characteristics, 1)
    IF service.uuid = services(accel%) THEN
    ! Found the accelerometer.
    print characteristics(i).uuid
    SELECT CASE characteristics(i).uuid
      CASE "FFF1"
        ! Tell the CC2650 to begin sending data.
        IF debug THEN PRINT "Write Command"
        DIM value(1) as INTEGER
        value(1) = modecode
    
        peripheral.writeCharacteristic(characteristics(i), value, 1)
        connected=1
        !peripheral.setNotify(characteristics(i), 1)
        peripheral.readCharacteristic(characteristics(i))
    
    
      CASE "FFF5"
      !Used to recieve the actual wmmu fft data
      IF debug THEN PRINT "RXing FFT Data"
      DIM RXData(1) as INTEGER
      !peripheral.setNotify(characteristics(i), 1)
      peripheral.readCharacteristic(characteristics(i))
    
      CASE "F000AA12" & servicesHeader
        ! Turn the accelerometer sensor on.
        IF debug THEN PRINT "Accelerometer on."
        DIM value(1) as INTEGER
        value(1) = 1
        peripheral.writeCharacteristic(characteristics(i), value, 1)
    
      CASE "F000AA13" & servicesHeader
        ! Set the sample rate to 500ms.
        DIM value(1) as INTEGER
        value(1) = 50
        IF debug THEN PRINT "Setting accelerometer sample rate to "; value(1)
        peripheral.writeCharacteristic(characteristics(i), value, 1)
    END SELECT
    END IF
    NEXT
    END IF
    END SUB
    
    
    ! Called to return information from a characteristic.
    !
    ! Parameters:
    !    time - The time when the information was received.
    !    peripheral - The peripheral.
    !    characteristic - The characteristic whose information
    !        changed.
    !    kind - The kind of call. One of
    !        1 - Called after a discoverDescriptors call.
    !        2 - Called after a readCharacteristics call.
    !        3 - Called to report status after a writeCharacteristics
    !            call.
    !    message - For errors, a human-readable error message.
    !    err - If there was an error, the Apple error number. If there
    !        was no error, this value is 0.
    !
    SUB BLECharacteristicInfo (time AS DOUBLE, _
                          peripheral AS BLEPeripheral, _
                          characteristic AS BLECharacteristic, _
                          kind AS INTEGER, _
                          message AS STRING, _
                          err AS LONG)
    IF kind = 2 THEN
    DIM value(1) AS INTEGER
    
    value = characteristic.value
    !input line$
    
    SELECT CASE characteristic.uuid
    CASE "FFF1"
    ! Update the accelerometer.
    
    
    !  IF value(1) = 94 THEN
    !  value(1) = 93
    !  ELSE
    !      value(1) = 94
    !  print value(1)
    !    print RXData
    
    !  END IF
    
    value(1) = modecode
    peripheral.writeCharacteristic(characteristic, value, 1)
    peripheral.readCharacteristic(characteristic)
    
    !delay = 0.2
    
    CASE "FFF5"
    ! RX FFT Data
    
    print value(1)
    !print RXData
    
    IF zTemp < 400 THEN
    
    IF value(1) = 0 THEN
        zTemp = 1
    END IF
    
    IF abs(firstvalue - value(1)) > 0 THEN
          print value(2)
            firstvalue=value(1)
            value(1)=value(2)
      FOR x = 1 TO 20
      !print value(x)
    zDataBuff(zTemp, 2) = value(x)
    zTemp = zTemp + 1
    NEXT
    
    
    
    END IF
    
    ELSE
    setUpGUI
    zTemp = 1
    
    END IF
    peripheral.readCharacteristic(characteristic)
    
    END SELECT
    ELSE IF kind = 3 AND err <> 0 THEN
    PRINT "Error writing "; characteristic.uuid; ": ("; err; ") "; message
    END IF
    END SUB
    
    
    
    !SUB nullEvent (time AS DOUBLE)
    !      IF connected = 1 THEN
    !        DIM characteristics(1) AS BLECharacteristic
    !  characteristics = WMMURadio.characteristics(1)
    !  FOR i = 1 TO UBOUND(characteristics, 1)
    !      ! Found the accelerometer.
    !      IF chacteristics(i).uuid = "FFF1" THEN
    !          WMMURadio.readCharacteristic(characteristics(i))
    !      END IF
    !  NEXT
    !      END IF
    !END SUB
    
    ! Send the last recorded data file to an email.
    
    SUB sendData
    DIM e AS eMail
    e = System.newEMail
    IF e.canSendMail THEN
    e.setSubject("Accelerometer data")
    e.setMessage("Accelerometer data")
    e.addAttachment(fileName$, "text/plain")
    e.send
    ELSE
    button = Graphics.showAlert("Can't Send", _
      "Email cannot be sent from this device.")
    END IF
    END SUB
    
    
    
    ! Creates a new button with a gradient fill.
    !
    ! Parameters:
    !    x - Horizontal location.
    !    y - Vertical location.
    !    title - Name of the button.
    !
    ! Returns: The new button.
    
    FUNCTION newButton (x, y, title AS STRING) AS Button
    DIM b AS Button
    b = Graphics.newButton(x, y)
    b.setTitle(title)
    b.setBackgroundColor(1, 1, 1)
    b.setGradientColor(0.6, 0.6, 0.6)
    newButton = b
    END FUNCTION
    
    
    
    
    ! Set up the user interface.
    
    SUB setUpGUI
    ! Tell the accelerometer to update once every 0.05 seconds.
    sensors.setAccelRate(0.05)
    
    ! Initialize the plot arrays.
    FOR t = 1 TO 400
    zDataBuff(t, 1) = t
    NEXT
    
    ! Initialize the plot and show it.
    p = Graphics.newPlot
    p.setTitle("WMMU GRAPH DATA")
    p.setXAxisLabel("Sample Number (X 2.4 = Hertz)")
    p.setYAxisLabel("Magnitude")
    p.showGrid(1)
    p.setGridColor(0.8, 0.8, 0.8)
    p.setAllowedGestures($0042)
    
    px = p.newPlot(zDataBuff)
    px.setColor(0, 1, 0)
    px.setPointColor(0, 1, 0)
    
    ! Set the plot range and domain. This must be done
    ! after adding the first PlotPoint, since that also
    ! sets the range and domain.
    p.setView(0, -1, 400, 256, 0)
    
    ! Show the graphics screen. Pass 1 as the parameter
    ! for full-screen mode.
    system.showGraphics(1)
    
    ! Lock the screen in the current orientation.
    orientation = 1 << (System.orientation - 1)
    System.setAllowedOrientations(orientation)
    
    ! Set the plot size.
    p.setRect(0, 0, Graphics.width, Graphics.height - 47)
    
    ! Draw the background.
    Graphics.setPixelGraphics(0)
    Graphics.setColor(0.886, 0.886, 0.886)
    Graphics.fillRect(0, 0, Graphics.width, Graphics.height)
    
    ! Set up the user interface.
    h = Graphics.height - 47
    quit = newButton(Graphics.width - 82, h, "Quit")
    send = newButton(Graphics.width - 266, h, "Send")
    samples = newButton(Graphics.width - 466, h, "Samples")
    fourier = newButton(Graphics.width - 566, h, "FFT(0-1KHz")
    nextKHz =  newButton(Graphics.width - 666, h, "FFT(1-2KHz)")
    nextKHz2 =  newButton(Graphics.width - 766, h, "FFT(2-3KHz)")
    nextKHz3 =  newButton(Graphics.width - 866, h, "FFT(3-4KHz)")
    nextKHz4 =  newButton(Graphics.width - 966, h, "FFT(4-5KHz)")
    
    ! If there is nothing to send, disable the Send button.
    IF NOT EXISTS(fileName$) THEN
    send.setEnabled(0)
    END IF
    END SUB
    
    
    ! Handle a tap on one of the buttons.
    !
    ! Parameters:
    !    ctrl - The button that was tapped.
    !    time - The time when the event occurred.
    
    SUB touchUpInside (ctrl AS Button, time AS DOUBLE)
    IF ctrl = quit THEN
    STOP
    ELSE IF ctrl = send THEN
    sendData
    ELSE IF ctrl = samples THEN
    modecode = 93
    ELSE IF ctrl = fourier THEN
    modecode = 94
    ELSE IF ctrl = nextKHz THEN
    modecode = 92
    ELSE IF ctrl = nextKHz2 THEN
    modecode = 91
    ELSE IF ctrl = nextKHz3 THEN
    modecode = 90
    ELSE IF ctrl = nextKHz4 THEN
    modecode = 89
    END IF
    END SUB
    

    Hi,

    Please see the source code in the attached file.

    -Nathan

  • Thanks Nathan,

    Very helpful.

    Kind Regards,
    Tibor

**Attention** This is a public forum