Hello
My customer us having problems with Port 2 of the MSP432P401R and tells me
We seem to have an issue that we can only pin down to the processor.
We have three LEDs on Port 2.0, 2.1 and 2.2.
We have I2C configured on UCB1. Whenever we receive a byte the LED on port 2.0 comes on, when we have finished with the data (no more bytes), we turn it off.
We are finding that the LED, even though it has been told to turn off, will stay on, about 20% of the time.
We have confirmed this is not a problem with the code by toggling other lines high and low, it is only on this port that it happens, for all LEDs.
Do you know if this is a known issue or what might cause this?
They are aware of Errata "PORT31" and have it as a standard driven (not high drive) GPIO and in output mode. This seems to be the state that it should work in, but it doesn’t. They also have all the other pins on that port as outputs and driven low – as recommended.
Best Regards
Bob Bacon