Part Number: MSP430G2553
Hi all:
I am having trouble figuring out this problem. Maybe someone here can give me some ideas. I am using the TI MSP430 Launchpad.
I have fixed the MSP430G2553 clock speed at 8 MHz in the code, and according to the datasheet, the clock speed should increase with increasing voltage. However, when I measure it using DCO calibration technique, I get a decreasing clock speed with increasing voltage. The variation is not too much; it varies between 7.92 to 8.16MHz. But shouldn't it be fixed at 8MHz, or maybe increase? I see nothing in the datasheet that explains this anomaly.
Any ideas?