Other Parts Discussed in Thread: MSP430FR6989, MSP430FR5994, MSP430FR5969, MSP-EXP430FR6989
Hi all
I need some help and advise please. To start it should be noted that I am in no way familiar with anything technical so please speak to me in lamens terms. All I have is an idea of what I want to achieve but have no idea how it would work or if its feasible from a business point of view.
Here in Cyprus during the winter we need to switch on our hot water boilers and wait 30 min - 1hr to have hot water before we can shower. The installation for the water boilers is simple. The water boiler is connected to the main Distribution board and then the power from the DB goes to the relay switch on the wall inside the house which you need to switch on and off like a light switch. the power we use here is 240V
I would like to be able to control this remotely via an app. The IT guys I have here have pointed me in the direction of the MSP430 Launchpad and say they can develop the software to control the device if needed.
Would this be the correct product for me to use?
If so how would the install work?
Thank you for your help