Part Number: MSP430F5438A
Other Parts Discussed in Thread: MSP-FET
Hi!
I have an application where I need a PWM output while the system is in LPM3. Thanks to a low frequency requirement I use ACLK=XT1 (which is already in use for RTC) as clock source.
When I run the pwm via a timer (in this case TA1) with ACLK as clock source the timer stops operating UNLESS I set SMCLKOFF=0 - this is weird as SMCLK is NOT the timer clock source and there is also no hint in the errata.