This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F5438: temperature accuracy

Part Number: MSP430F5438


Hi

What's the integrated temperature accuracy? It's not mentioned on datasheet.

Can it meet ±2℃? How about it's consistency performance in mass production?

  • Hi Daniel,

    If you mean the integrated temperature sensor, the accuracy is defined in the User guide, page 83. The TLV values are written at 30 and 85C with an accuracy of +/-3C. This is the worst case which you achieve using the calibration (TLV) data.
    However, you can calibrate your device (2 point calibration) to achieve better accuracy.

    Best regards
    Lukas

**Attention** This is a public forum