Part Number: MSP432P401R
Need a little help. I'm been trying to use the driverlib example I2C repeat start program to connect to a Si7051x temperature chip with very little luck.
Problem 1: Only able to sample I2C on logic analyzer after pushing reset button. When capturing immediately after pushing the reset, this is what I get from analyzer.
The measure sequence for the Si7051 w/o clockstretching is on page 14 of this document.
http://www.silabs.com/documents/public/data-sheets/Si7050-1-3-4-5-A20.pdf
Problem 2: Stopping at following line when pausing debug. Looks as if nothing is going into the TXBUF
//Poll for transmit interrupt flag.
while (!BITBAND_PERI(EUSCI_B_CMSIS(moduleInstance)->rIFG.r, UCTXIFG_OFS))
The code I'm using is below: Thanks for the help.
#include "driverlib.h"
/* Standard Defines */
#include <stdint.h>
#include <stdbool.h>
#include <string.h>
#include <Si7051.h>
/* Slave Address for I2C Slave */
#define SLAVE_ADDRESS IC_ADDRESS_TMP7051_ADDRESS
#define NUM_OF_REC_BYTES 2
/* Variables */
//const uint8_t TXData[2] = 0;
static uint8_t RXData[NUM_OF_REC_BYTES];
static volatile uint32_t xferIndex;
static volatile bool stopSent;
/* I2C Master Configuration Parameter */
const eUSCI_I2C_MasterConfig i2cConfig =
{
EUSCI_B_I2C_CLOCKSOURCE_SMCLK, // SMCLK Clock Source
3000000, // SMCLK = 3MHz
EUSCI_B_I2C_SET_DATA_RATE_100KBPS, // Desired I2C Clock of 100khz
0, // No byte counter threshold
EUSCI_B_I2C_NO_AUTO_STOP // No Autostop
};
int main(void)
{
static volatile uint32_t ii;
/* Disabling the Watchdog */
MAP_WDT_A_holdTimer();
/* Select Port 1 for I2C - Set Pin 6, 7 to input Primary Module Function,
* (UCB0SIMO/UCB0SDA, UCB0SOMI/UCB0SCL).
*/
MAP_GPIO_setAsPeripheralModuleFunctionInputPin(GPIO_PORT_P1,
GPIO_PIN6 + GPIO_PIN7, GPIO_PRIMARY_MODULE_FUNCTION);
//stopSent = false;
memset(RXData, 0x00, NUM_OF_REC_BYTES);
/* Initializing I2C Master to SMCLK at 100khz with no autostop */
MAP_I2C_initMaster(EUSCI_B0_BASE, &i2cConfig);
/* Specify slave address */
MAP_I2C_setSlaveAddress(EUSCI_B0_BASE, SLAVE_ADDRESS);
/* Set Master in transmit mode */
MAP_I2C_setMode(EUSCI_B0_BASE, EUSCI_B_I2C_TRANSMIT_MODE);
/* Enable I2C Module to start operations */
MAP_I2C_enableModule(EUSCI_B0_BASE);
/* Enable and clear the interrupt flag */
MAP_I2C_clearInterruptFlag(EUSCI_B0_BASE, EUSCI_B_I2C_RECEIVE_INTERRUPT0);
MAP_I2C_clearInterruptFlag(EUSCI_B0_BASE, EUSCI_B_I2C_NAK_INTERRUPT);
MAP_I2C_clearInterruptFlag(EUSCI_B0_BASE, EUSCI_B_I2C_TRANSMIT_INTERRUPT0);
//Enable master Transmit interrupt
MAP_I2C_enableInterrupt(EUSCI_B0_BASE, EUSCI_B_I2C_NAK_INTERRUPT);
MAP_I2C_enableInterrupt(EUSCI_B0_BASE, EUSCI_B_I2C_RECEIVE_INTERRUPT0);
MAP_I2C_enableInterrupt(EUSCI_B0_BASE, EUSCI_B_I2C_TRANSMIT_INTERRUPT0);
MAP_Interrupt_enableSleepOnIsrExit();
MAP_Interrupt_enableInterrupt(INT_EUSCIB0);
while (1)
{
MAP_I2C_enableInterrupt(EUSCI_B0_BASE, EUSCI_B_I2C_TRANSMIT_INTERRUPT0);
//MAP_I2C_enableInterrupt(EUSCI_B0_BASE, EUSCI_B_I2C_RECEIVE_INTERRUPT0);
/* Making sure the last transaction has been completely sent out */
while (MAP_I2C_masterIsStopSent(EUSCI_B0_BASE) == EUSCI_B_I2C_SENDING_STOP);
/* Send start and the first byte of the transmit buffer. We have to send
* two bytes to clean out whatever is in the buffer from a previous
* send */
//MAP_I2C_masterSendSingleByte(EUSCI_B0_BASE, MEAS_TEMP_HOLD_REGISTER);
while (MAP_I2C_isBusBusy(EUSCI_B0_BASE) == EUSCI_B_I2C_BUS_BUSY);
// {
MAP_I2C_masterSendStart(EUSCI_B0_BASE);
MAP_I2C_masterSendMultiByteStart(EUSCI_B0_BASE, MEAS_TEMP_NOHOLD_REGISTER);
MAP_I2C_masterSendMultiByteNext(EUSCI_B0_BASE, MEAS_TEMP_NOHOLD_REGISTER);
/* Enabling transfer interrupt after stop has been sent */
MAP_I2C_enableInterrupt(EUSCI_B0_BASE, EUSCI_B_I2C_TRANSMIT_INTERRUPT0 + EUSCI_B_I2C_RECEIVE_INTERRUPT0);
//MAP_Interrupt_enableSleepOnIsrExit();
//MAP_PCM_gotoLPM0InterruptSafe();
/* While the stop condition hasn't been sent out... */
// while(!stopSent)
//{
//MAP_PCM_gotoLPM0InterruptSafe();
//}
//stopSent = false;
/* Delay between Transmissions */
}
}
/*******************************************************************************
* eUSCIB0 ISR. The repeated start and transmit/receive operations happen
* within this ISR.
*******************************************************************************/
void EUSCIB0_IRQHandler(void)
{
uint_fast16_t status;
status = MAP_I2C_getEnabledInterruptStatus(EUSCI_B0_BASE);
MAP_I2C_clearInterruptFlag(EUSCI_B0_BASE, status);
// if (status & EUSCI_B_I2C_NAK_INTERRUPT)
// {
//MAP_I2C_masterSendSingleByte(EUSCI_B0_BASE, MEAS_TEMP_NOHOLD_REGISTER);
// }
/* If we reached the transmit interrupt, it means we are at index 1 of
* the transmit buffer. When doing a repeated start, before we reach the
* last byte we will need to change the mode to receive mode, set the start
* condition send bit, and then load the final byte into the TXBUF.
*/
if (status & EUSCI_B_I2C_TRANSMIT_INTERRUPT0)
{
//MAP_I2C_masterSendSingleByte(EUSCI_B0_BASE, MEAS_TEMP_HOLD_REGISTER);
MAP_I2C_masterSendMultiByteNext(EUSCI_B0_BASE, MEAS_TEMP_NOHOLD_REGISTER);
MAP_I2C_disableInterrupt(EUSCI_B0_BASE, EUSCI_B_I2C_TRANSMIT_INTERRUPT0);
MAP_I2C_setMode(EUSCI_B0_BASE, EUSCI_B_I2C_RECEIVE_MODE);
xferIndex = 0;
MAP_I2C_masterReceiveStart(EUSCI_B0_BASE);
MAP_I2C_enableInterrupt(EUSCI_B0_BASE, EUSCI_B_I2C_RECEIVE_INTERRUPT0);
//MAP_I2C_masterReceiveMultiByteNext(EUSCI_B0_BASE);
}
/* Receives bytes into the receive buffer. If we have received all bytes,
* send a STOP condition */
if (status & EUSCI_B_I2C_RECEIVE_INTERRUPT0)
{
if(xferIndex == NUM_OF_REC_BYTES - 2)
{
MAP_I2C_masterReceiveMultiByteStop(EUSCI_B0_BASE);
RXData[0] = MAP_I2C_masterReceiveMultiByteNext(EUSCI_B0_BASE);
xferIndex++;
}
else if(xferIndex == NUM_OF_REC_BYTES - 1)
{
RXData[1] = MAP_I2C_masterReceiveMultiByteNext(EUSCI_B0_BASE);
MAP_I2C_disableInterrupt(EUSCI_B0_BASE, EUSCI_B_I2C_RECEIVE_INTERRUPT0);
MAP_I2C_setMode(EUSCI_B0_BASE, EUSCI_B_I2C_TRANSMIT_MODE);
xferIndex = 0;
//stopSent = true;
//MAP_Interrupt_disableSleepOnIsrExit();
}
else
{
RXData[xferIndex++] = MAP_I2C_masterReceiveMultiByteNext(EUSCI_B0_BASE);
}
}
}