This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

msp430f5659: ADC ISR routine not working

Part Number: MSP430F5659
Other Parts Discussed in Thread: MSP430F5659

hello,

I am usinf msp430f5659 and trying to interface adc on pin p6.2. I have intialized adc but it is not converting anlog voltage. I have maximum voltage of 3.3 on p6.2. I have 4MHz smclk. It is not entering into ISR. Please help me to find the problem.

My code is:

void adc_configure()
{
    P6SEL |= BIT2;                                    // selecting bit0 as analog input pin
    ADC12CTL0 &= ~ ADC12ENC;
      REFCTL0 &= ~REFMSTR;                      // Reset REFMSTR to hand over control to
                                                // ADC12_A ref control registers
    ADC12CTL0 |= ADC12ON + ADC12SHT0_12 + ADC12MSC + ADC12REFON + ADC12REF2_5V;    // To on ADC10,Reference on, 1024 ADC12CLK cycles
    ADC12CTL1 |= ADC12DIV_7 + ADC12SSEL_3;    // ADC12SC sample and hold source, Stright binary format, /8 clock divider, clk source= SMCLK, Single channel signal conversion, no operation is active
    ADC12CTL2 |= ADC12RES_1 +  ADC12PDIV;          //ADC12_A resolution 10 bit (11 clock cycle conversion time), ADC12_A predivider/4
    ADC12MCTL0 = ADC12SREF_1 + ADC12INCH_2;        //selected ref = vcc and vss, selected channel= A2
    ADC12IE |= ADC12IE0 ;                                 // ADC_IFG upon conv result-ADCMEMO
    ADC12CTL0 |= ADC12ENC;                         // To start sample and conversion, to enable ADC12
    __bis_SR_register(GIE);
}

#pragma vector= ADC12_VECTOR
__interrupt void ADC12_ISR(void)
{
   while (!(ADC12IFG & BIT0));
     __bic_SR_register_on_exit(CPUOFF);
}

this is in my main function :

ADC12CTL0 |= ADC12SC + ADC12ENC ;           // To start sample and conversion, to enable ADC10

adc12_value = (float)ADC12MEM0;
sprintf(string,"%3.2f",adc12_value);

  • harish yadav,

    P6.2 is Channel A2. So you need to enable ADC12IE2 and read ADC12MEM2. And check (ADC12IFG & BIT2) as well.

    Regards,
    Ling
  • I tried this also but it is not working. I found that it is not entering into the Interrupt service routine.
  • #include <msp430.h>
    
    volatile unsigned int results;           // Needs to be global in this example
    
    int main(void)
    {
      WDTCTL = WDTPW+WDTHOLD;                   // Stop watchdog timer
      P6SEL = BIT2;                             // Enable A/D channel inputs
      REFCTL0 &= ~REFMSTR;                      // Reset REFMSTR to hand over control to
                                                // ADC12_A ref control registers
      ADC12CTL0 = ADC12ON+ADC12SHT02+ADC12REFON+ADC12REF2_5V;
      ADC12CTL1 = ADC12SHP;                     // Use sampling timer
      ADC12MCTL0 = ADC12SREF_1 + ADC12INCH_2;   // Vr+=Vref+ and Vr-=AVss, channel = A2
      ADC12IE = BIT0;                           // Enable ADC12IFG.0
      ADC12CTL0 |= ADC12ENC;                    // Enable conversions
    
      while(1)
      {
        ADC12CTL0 |= ADC12SC;
        __bis_SR_register(LPM0_bits + GIE);     // Enter LPM0, Enable interrupts
        __no_operation();                       // For debugger    
      }
    }
    
    #if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
    #pragma vector=ADC12_VECTOR
    __interrupt void ADC12ISR (void)
    #elif defined(__GNUC__)
    void __attribute__ ((interrupt(ADC12_VECTOR))) ADC12ISR (void)
    #else
    #error Compiler not supported!
    #endif
    {
        switch(__even_in_range(ADC12IV,34))
      {
      case  0: break;                           // Vector  0:  No interrupt
      case  2: break;                           // Vector  2:  ADC overflow
      case  4: break;                           // Vector  4:  ADC timing overflow
      case  6:                                  // Vector  6:  ADC12IFG0
          results = ADC12MEM0;               // Move results, IFG is cleared
          __bic_SR_register_on_exit(LPM0_bits); // Exit active CPU, SET BREAKPOINT HERE
      break;
      case  8: break;                           // Vector  8:  ADC12IFG1
      case 10: break;                           // Vector 10:  ADC12IFG2
      case 12: break;                           // Vector 12:  ADC12IFG3
    
      case 14: break;                           // Vector 14:  ADC12IFG4
      case 16: break;                           // Vector 16:  ADC12IFG5
      case 18: break;                           // Vector 18:  ADC12IFG6
      case 20: break;                           // Vector 20:  ADC12IFG7
      case 22: break;                           // Vector 22:  ADC12IFG8
      case 24: break;                           // Vector 24:  ADC12IFG9
      case 26: break;                           // Vector 26:  ADC12IFG10
      case 28: break;                           // Vector 28:  ADC12IFG11
      case 30: break;                           // Vector 30:  ADC12IFG12
      case 32: break;                           // Vector 32:  ADC12IFG13
      case 34: break;                           // Vector 34:  ADC12IFG14
      default: break; 
      }
    }
    
    

  • Hi harish yadav,

    Have you solved the problem?

    Regards,
    Ling

**Attention** This is a public forum