This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/msp430f6435: unable to clear oscillator fault flag

Part Number: MSP430F6435


Tool/software: Code Composer Studio

Hi,I used the following way for msp430 clock initialization .

***********************************************************************************

while(BAKCTL & LOCKBAK)                    // Unlock XT1 pins for operation
     BAKCTL &= ~(LOCKBAK);

  UCSCTL6 &= ~(XT1OFF);                     // XT1 On
  UCSCTL6 |= XCAP_3;                        // Internal load cap

  // Loop until XT1,XT2 & DCO stabilizes - In this case loop until XT1 and DCo settle
  do
  {
    UCSCTL7 &= ~(XT2OFFG + XT1LFOFFG + DCOFFG);
                                            // Clear XT2,XT1,DCO fault flags
    SFRIFG1 &= ~OFIFG;                      // Clear fault flags
  }while (SFRIFG1&OFIFG);                   // Test oscillator fault flag

**********************************************************************************

the program execution is not coming out of do_while loop which indicates that oscillator fault flag is not cleared .How to resolve this issue??

**Attention** This is a public forum