This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F6779: SYS module with Fast Vcc

Expert 2355 points
Part Number: MSP430F6779


MSP430F67xx has BOR with Device Errata SYS16.

It describes as below:

SYS16

At initial power-up, after Vcc crosses the bownout threshold and reaches

a constant level, an abrupt ramp of Vcc at a rate dV/dT > 1V/100us can cause

a brownout condition to be incorrectly detected even though Vcc does not

fall below the brownout threshold.

 

So,I have a question about ramp up speed.

Is it possible to cause a reset when the inclination of dV/dT also exceeds this price in less than 1 V of fluctuation?

(i.e:0.95V / 95 usec)

best regards,

kyt

**Attention** This is a public forum