Part Number: MSP430FR5969
Dear All;
I don't think the dimensions in the packaging information are in error. Or I'm not understanding the dimension system of TI. The datasheet mentions that they are all in 'milimeters'. But the seem to be too small. Below is MSP430FR5969's dimension information. Is the width and the height only 7.8mm? That seems to be really small. And also the pitch distance is "44 x 0.50", what does this mean?
Also, what are these dimensions 6.15 over 5.85?
Please enlighten me.....
Best regards,
Suh, Sukho