Team, I am currently attempting to use an MSP430F5529 to read in an analog value and populate it to an array. I have configured the MSP430 to start a sample conversion off of TimerA0, as shown in the datasheet, but am currently getting no response from the ADC. Please see my code below. Any advice on what I'm configuring incorrectly would be much appreciated
#include <msp430.h>
static void setup_ADC();
void setup_TimerA0(void);
void setClocks();
void SetVcoreUp (unsigned int level);
#define Num_of_Results 2000
volatile unsigned int results[Num_of_Results]; //stores 500 words, or at an optimal sampling of 100ksps of 1kHz sine,
//5 periods worth of data
unsigned char index = 0;
void main(void) {
WDTCTL = WDTPW | WDTHOLD; // Stop watchdog timer
setClocks(); //set ACLK to REF0 = 32.768KHz, MCLK and SMCLK to DCO = 20MHz
setup_TimerA0();
setup_ADC();
infinite_loop:
{
__bis_SR_register(GIE); // LPM0, global interrupts enabled
__no_operation(); // For debugger
}
goto infinite_loop;
}
// Functions //
// Timer1 interrupt service routine
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=TIMER1_A0_VECTOR
__interrupt void TIMER1_A0_ISR(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(TIMER1_A0_VECTOR))) TIMER1_A0_ISR (void)
#else
#error Compiler not supported!
#endif
{
P1OUT ^= 0x01; // Toggle P1.0
TA1CCR0 += 50000; // Add Offset to CCR0
}
//ADC Interrupt
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=ADC12_VECTOR
__interrupt void ADC12ISR (void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(ADC12_VECTOR))) ADC12ISR (void)
#else
#error Compiler not supported!
#endif
{
results[index] = ADC12MEM0; // Move results
index++; // Increment results index, modulo; Set Breakpoint1 here
if (index == 2000)
index = 0;
ADC12IFG = 0x0000;
}
static void setup_ADC(void){
/* Output impedance of the DAC buffer (OPA735) is 125 ohms, so from section 28.2.5.3 of the user's guide
* t_samp > (125+1800)*2^13*25p + 800n, or t_samp > 1.234us. MCLK/4 period is 200ns,
* so needed sample period is 7 clocks (?)
*/
ADC12CTL0 = ADC12SHT0_1 | ADC12ENC | ADC12ON; // Sampling timer is 8 clocks, enable conversions, turn ADC12 on
ADC12CTL1 = ADC12SSEL_2 | ADC12DIV_3 | ADC12SHS_1 | ADC12SHP; // MCLK (20MHz) chosen as reference clock
// Divide the clock by 4. New Clock becomes MCLK/4 = 5MHz
//SHI source is Timer A CCR1
//SAMPCON is sourced from sampling timer (8 clocks)
P6SEL |= 0x01; // P6.0 ADC channel A0 select
ADC12IE = 0x01; //Enable ADC Interrupts
}
void setClocks(void)
{
void SetVcoreUp (unsigned int level);
// Increase Vcore setting to level3 to support fsystem=20MHz
// NOTE: Change core voltage one level at a time..
SetVcoreUp (0x01);
SetVcoreUp (0x02);
SetVcoreUp (0x03);
UCSCTL3 = SELREF_2; // Set DCO FLL reference = REFO
UCSCTL4 |= SELA_2; // Set ACLK = REFO
__bis_SR_register(SCG0); // Disable the FLL control loop
UCSCTL0 = 0x0000; // Set lowest possible DCOx, MODx
UCSCTL1 = DCORSEL_5; // Select DCO range 20MHz operation
UCSCTL2 = 610; // Set DCO Multiplier for 20MHz
// (N + 1) * FLLRef = Fdco
// (610 + 1) * 32768 = 20MHz
__bic_SR_register(SCG0); // Enable the FLL control loop
// Worst-case settling time for the DCO when the DCO range bits have been
// changed is n x 32 x 32 x f_MCLK / f_FLL_reference. See UCS chapter in 5xx
// UG for optimization.
// 32 x 32 x 25 MHz / 32,768 Hz ~ 780k MCLK cycles for DCO to settle
__delay_cycles(625000);
// Loop until XT1,XT2 & DCO stabilizes - In this case only DCO has to stabilize
do
{
UCSCTL7 &= ~(XT2OFFG + XT1LFOFFG + DCOFFG);
// Clear XT2,XT1,DCO fault flags
SFRIFG1 &= ~OFIFG; // Clear fault flags
}while (SFRIFG1&OFIFG); // Test oscillator fault flag
}
void SetVcoreUp (unsigned int level)
{
// Open PMM registers for write
PMMCTL0_H = PMMPW_H;
// Set SVS/SVM high side new level
SVSMHCTL = SVSHE + SVSHRVL0 * level + SVMHE + SVSMHRRL0 * level;
// Set SVM low side to new level
SVSMLCTL = SVSLE + SVMLE + SVSMLRRL0 * level;
// Wait till SVM is settled
while ((PMMIFG & SVSMLDLYIFG) == 0);
// Clear already set flags
PMMIFG &= ~(SVMLVLRIFG + SVMLIFG);
// Set VCore to new level
PMMCTL0_L = PMMCOREV0 * level;
// Wait till new level reached
if ((PMMIFG & SVMLIFG))
while ((PMMIFG & SVMLVLRIFG) == 0);
// Set SVS/SVM low side to new level
SVSMLCTL = SVSLE + SVSLRVL0 * level + SVMLE + SVSMLRRL0 * level;
// Lock PMM registers for write access
PMMCTL0_H = 0x00;
}
void setup_TimerA0(void){
TA0CTL = TASSEL_2 + MC_1; // SMCLK, up mode, clear TAR
TA0CCR0 = 200-1; //200 clocks@5MHz = 100ksps
TA0CCTL1 = OUTMOD_3; //Set, Reset on TA1
TA0CCR1 = 99; //trigger for ADC
//Code to examine sample PW cycle at GPIO
P1SEL |= BIT2; // P1.2 option select
P1DIR |= BIT2; // P1.2 output
}