Part Number: MSP430FR5949
Tool/software: Code Composer Studio
Hi,
I'm starting to develop a fairly simple code for MSP430FR5949. I started by creating some functions libraries and then the main file. After some basic configurations (which I still not know very well), imported from other projects, I call some functions to configure the RTC current time, i2c pins, etc. Thing is: the MSP stops when calling any of these functions. I've put breakpoints whenever I call any functions and on each function's first line, and realized that the MSP seems to call the function, but do not execute the function first line, it goes somewhere esse instead. When I pause the execution, most of the times it is at ZI_FUNCTION, stuck at the loop while at the last line. I can't understand why it cannot call any function properly.
Code:
#include <msp430.h>
#include <stdio.h>
#include <string.h>
#include "serial.h"
#include "serialparalelo.h"
#include "i2c.h"
#include "controlador.h"
volatile uint16_t cont_timeout_rx;
volatile uint16_t ind_rx0, ind_rx1, cont_rx0, cont_rx1;
volatile uint8_t uart = 1;
volatile uint8_t rx0_buff[tmn_buffer_rx0], rx1_buff[tmn_buffer_rx1];
// RTC
uint8_t current_time[6] = {0,0,0,0,0,0};
// I2C variable
volatile uint16_t i2c_timeout = 0;
// Variaveis noinit e persistent na FRAM
#pragma SET_DATA_SECTION(".TI.noinit")
Controle controlador;
#pragma SET_DATA_SECTION(".TI.persistent")
volatile uint16_t counter_plan = 0;
#pragma SET_DATA_SECTION()
#pragma vector = TIMER0_A0_VECTOR
__interrupt void Timer_A (void)
{
if(counter_plan)
counter_plan--;
if(i2c_timeout)
i2c_timeout--;
}
// Timer B0
#pragma vector = TIMER0_B0_VECTOR
__interrupt void Timer_B0_ISR (void)
{
TB0CTL &= ~(TBIE);
}
// UART 0
#pragma vector = USCI_A0_VECTOR
__interrupt void USCI_A0_ISR(void) // MODEM
{
UCA0IFG &= ~UCRXIFG; // Clear interrupt
rx0_buff[ind_rx0]=UCA0RXBUF;
ind_rx0++;
if(ind_rx0==tmn_buffer_rx0)
ind_rx0=0;
cont_timeout_rx=0; // limpa o cont_time_rx
}
// UART 1
#pragma vector = USCI_A1_VECTOR
__interrupt void USCI_A1_ISR(void) //USB
{
UCA1IFG &=~ UCRXIFG; // Clear interrupt
rx1_buff[ind_rx1]=UCA1RXBUF;
ind_rx1++;
if(ind_rx1==tmn_buffer_rx1)
ind_rx1=0;
cont_timeout_rx=0;
}
// Functions
void set_time()
{
RTCCTL01 |= RTCHOLD; // Stop RTC calendar
RTCYEAR = current_time[2]; // Year
RTCMON = current_time[1]; // Month
RTCDAY = current_time[0]; // Day
//RTCDOW = 0x01; // Day of week = 0x01 = Monday
RTCHOUR = current_time[3]; // Hour
RTCMIN = current_time[4]; // Minute
RTCSEC = current_time[5]; // Seconds
RTCCTL01 &= ~(RTCHOLD); // Start RTC calendar mode
}
///////////////////////////////////////////////////////////////////////////
void get_time(void)
{
while(!(RTCCTL01 & RTCRDY));
current_time[2] = RTCYEAR; // Year
current_time[1] = RTCMON; // Month
current_time[0] = RTCDAY; // Day
// RTCDOW = 0x01; // Day of week = 0x01 = Monday
current_time[3] = RTCHOUR; // Hour
current_time[4] = RTCMIN; // Minute
current_time[5] = RTCSEC; // Seconds
}
int main(void)
{
WDTCTL = WDTPW + WDTHOLD; // Stop WDT
PM5CTL0 &= ~LOCKLPM5;
// FRAM Configuração
//FRCTL0_H = 0XA5; // Unlock FRAM registers
//FRCTL0_L = NWAITS0;
//FRCTL0_H = 0;
//Clock Configuration
CSCTL0_H = 0xA5; // Unlock clock registers
CSCTL1 = DCOFSEL_3 | DCORSEL; // Set DCO to 8MHz
CSCTL2 = SELA__LFXTCLK | SELS__DCOCLK | SELM__DCOCLK; // ACLK = SMCLK = MCLK = DCO
CSCTL3 = DIVA__1 | DIVS__1 | DIVM__1; // f(ACLK)/1; f(SMCLK)/1; f(MCLK)/1
CSCTL0_H = 0; // Lock CS registers
//---
/* Px.7 Px.6 Px.5 Px.4 Px.3 Px.2 Px.1 Px.0 */
PJDIR = 0b00000000;
P1DIR = 0b00000000;
P2DIR = 0b00000000;
P3DIR = 0b00000000;
// TimerA Configuration
TA0CCTL0 = CCIE | CAP; // TACCR0 interrupt enabled, compare mode
TA0CCR0 = 12500; // Timer A counts until 12500 (12500 = 100ms)
TA0CTL = TASSEL_2 | MC_1 | ID_3; // SMCLK, up mode, TCLK/8
TA0EX0 |= TAIDEX_7; // TCLK/8
// TimerB Configuration
TB0CCTL0 = CCIE; // TBCCR0 interrupt enabled
TB0CTL= MC_0;
// UART0 Configuration
P2SEL0 &= ~(BIT0 + BIT1); //Pins P2.0 e P2.1 as UART
P2SEL1 |= BIT0 + BIT1; //Pins P2.0 e P2.1 as UART
UCA0CTLW0 = UCSWRST; // Put eUSCI in reset
UCA0CTLW0 |= UCSSEL__SMCLK; // BRCLK = SMCLK
UCA0BR0 = 52; // int(BRCLK/16/9600)
UCA0BR1 = 0x00;
UCA0MCTLW |= UCOS16 | UCBRF_1;
UCA0CTLW0 &= ~UCSWRST; // Initialize eUSCI
UCA0IE |= UCRXIE; // Enable USCI_A1 RX interrupt
//---
// UART1 Configuration
P2SEL0 &= ~(BIT5 + BIT6); //Pins P2.5 e P2.6 as UART
P2SEL1 |= BIT5 + BIT6; //Pins P2.5 e P2.6 as UART
UCA1CTLW0 = UCSWRST; // Put eUSCI in reset
UCA1CTLW0 |= UCSSEL__SMCLK; // BRCLK = SMCLK
UCA1BR0 = 52; // int(BRCLK/16/9600)
UCA1BR1 = 0x00;
UCA1MCTLW |= UCOS16 | UCBRF_1;
UCA1CTLW0 &= ~UCSWRST; // Initialize eUSCI
UCA1IE |= UCRXIE; // Enable USCI_A1 RX interrupt
//RTC Configuration
PJSEL1 &= ~(BIT4 + BIT5);
PJSEL0 |= BIT4 + BIT5;
__bis_SR_register(GIE); // Habilita interrupção global
current_time[0] = 17;
current_time[1] = 1;
current_time[2] = 16;
current_time[3] = 19;
current_time[4] = 55;
current_time[5] = 00;
set_time(); // it usually stops execution here
i2c_init();
serialparalelo_init();
Code goes on...