Hi,
I am interfacing KENTEC K350 TFT display with the MSP432P401R EVM. The TFT display requires two power sources, 3.3 V & 5V. According to the datasheet the 5V is required for the display backlight. But I tried runninng it without the 5V supply and It was working fine. So I just wish to know what difference does it make and will it cause any damage to the TFT, if 5V is not provided.
Regards,
Amit K