This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F2618: MSP430 CC1101- AX.25 and SSP protocol programming.

Part Number: MSP430F2618

My graduation project has a MSP 430 micontroller connected from one end with a transciever through SPI and AX25 protocol and the other end with the on board computer through SSP and I2C protocols  .
I found sorces that explains AX,25 and SSP protocols but I am having programs with writing the code itself ( IAR ). Are there any good sources that explains AX.25 OR SSP protcols programming for microcontrollers from the start ? or even network programming in general for microcontrollers ? 

**Attention** This is a public forum