Part Number: MSP430F5528
Other Parts Discussed in Thread: MSP430F5529
Hi,
I needed to update the firmware of an existing product that uses FF29_USB_BSL_Flash.txt which has been customized with our VID/PID.
The update was on our application firmware only, and not on the bootloader, but it increased the size slightly and is now causing an overlap with the two bytes written at location @FFAE at the end of FF29_USB_BSL_Flash.txt.
I could really use some help figuring this out.
Thanks