Part Number: MSP430F5244
Tool/software: Code Composer Studio
Hi, I'm working on msp430F5244. My problem is when I run the controller at 1Mhz speed SPI works marginally and if I run the controller at 8Mhz SPI not at all working ,I pasted my code, Please help me someone where I'm wrong.
#include <msp430.h>
#include <stdint.h>
//#include "System_clk.h"
//#include "spi_function.h"
void systemClockConfigure_8Mhz()
{
PMAPPWD = 0x02D52; // Enable Write-access to modify port mapping registers
P4MAP7 = PM_MCLK;
PMAPPWD = 0; // Disable Write-Access to modify port mapping registers
UCSCTL3 = SELREF_2; // Set DCO FLL reference = REFO
UCSCTL4 |= SELA_2 /*| SELS__DCOCLK*/; // Set ACLK = REFO
__bis_SR_register(SCG0); // Disable the FLL control loop
UCSCTL0 = 0x0000; // Set lowest possible DCOx, MODx
UCSCTL1 = DCORSEL_5; // Select DCO range 16MHz operation
UCSCTL2 = FLLD_1 + 249; // Set DCO Multiplier for 8MHz
// (N + 1) * FLLRef = Fdco
// (249 + 1) * 32768 = 8MHz
__bic_SR_register(SCG0); // Enable the FLL control loop
// Worst-case settling time for the DCO when the DCO range bits have been
// changed is n x 32 x 32 x f_MCLK / f_FLL_reference. See UCS chapter in 5xx
// UG for optimization.
// 32 x 32 x 8 MHz / 32,768 Hz = 250000 = MCLK cycles for DCO to settle
__delay_cycles(250000);
// Loop until XT1,XT2 & DCO stabilizes - In this case only DCO has to stabilize
do
{
UCSCTL7 &= ~(XT2OFFG + XT1LFOFFG + DCOFFG);
// Clear XT2,XT1,DCO fault flags
SFRIFG1 &= ~OFIFG; // Clear fault flags
}while (SFRIFG1&OFIFG); // Test oscillator fault flag
UCSCTL4 |= SELS__DCOCLK | SELM__DCOCLK; //MCLK and SMCLK=DCOCLK
}
void systemClockConfigure_1Mhz()
{
PMAPPWD = 0x02D52; // Enable Write-access to modify port mapping registers
P4MAP7 = PM_MCLK;
PMAPPWD = 0; // Disable Write-Access to modify port mapping registers
UCSCTL4 |= SELA_2; // Set ACLK = REFO
}
void SPI_UCB1Init()
{
P4DIR |= BIT1 | BIT3 ;
P4SEL |= BIT1 | BIT3 ; // MISO and clk pin for spi
UCB1CTL1 |= UCSWRST;
UCB1CTL0 |= (UCMSB | UCSYNC | UCMST | UCCKPL); //3wire_spi + sync_mode + MSB first + master_mode UCCKPH | | UCCKPL
UCB1CTL1 |= UCSSEL__SMCLK; //SMCLK UCSSEL__SMCLK 12MHz
UCB1BR0 = 0x00;
UCB1BR1 = 0x00;
UCB1CTL1 &= ~UCSWRST;
}
void SPI_LCDTx(uint8_t value)
{
UCB1TXBUF=value;
while(!(UCB1IFG & UCTXIFG))
;
}
/*
* main.c
*/
int main(void) {
WDTCTL = WDTPW | WDTHOLD; // Stop watchdog timer
// systemClockConfigure_1Mhz();
systemClockConfigure_8Mhz();
SPI_UCB1Init();
while(1)
{
SPI_LCDTx('a');
SPI_LCDTx('b');
SPI_LCDTx('c');
}
return 0;
}