Part Number: MSP-FET430UIF
Tool/software: WEBENCH® Design Tools
Hi,
I'm trying to program M430FE425 Controller using MSP-FETU430IF, but the thing is I have only 7 pins on the controller board for programming.
now how can I identify those 7 pins on 14 pin JTag target on MSP-FETU430IF
The 7 pins on board are connected to controller as below:
pin1 connected to controller 62&63 pins
pin2 connected to controller 1&64 pins
pin3 connected to controller 59 pin
pin4 connected to controller 60 pin
pin5 connected to controller 57 pin
pin6 connected to controller 56 pin
pin7 connected to controller 55 pin
pin8 connected to controller 54 pin
pin9 connected to controller 58 pin
what are pins i have to use on jtag and how are the connected to those 9 pins
please help me on this please please
I would be glad if someone helps me....