Part Number: MSP432P401R
Hi,
I am using MSP432P401R EVM and interfacing MAX30100 using I2C. MAX30100 is an Pulse Oximeter Sensor. The I2C BUS goes busy indefinitely after transmission of 1st Byte to the Slave device. I have connected 10K pull up resistors on both the SDA and SCL lines and supplied with 3.3V to both. When I measured the Voltage at both the I2C lines, it showed 1.87V. Also i would mention that there is only one Slave Device i.e. Max30100.
Any help or suggestions?
Regards,
Amit Kotal