Part Number: MSP432P401R
Hi,
We are using the MSP432P401R controller in one of the Project it is went to EMI / EMC test, after this test we are observed the controller is Not functioning, and found Voltage on the Reset
pin is LOW, i tried to give the Reset by Applying the 3V on the Reset Pin, it is working some time and after that it going to the No functional state (i.e RESET pin is LOW) please suggest in which conditions the RESET pin Goes into LOW.
Thanks