Part Number: MSP432P401R
Tool/software: TI C/C++ Compiler
Hello! I'm trying to integrate the driver for W5500 Ethernet chip with my code on MSP432 controller, in Code Composer Studio 7 with latest updates. The driver can be found on GitHub. The problem is that the program will not compile because of a struct declaration in Ethernet/wizchip_conf.h. This is the declaration:
typedef struct __WIZCHIP
{
uint16_t if_mode; ///< host interface mode
uint8_t id[6]; ///< @b WIZCHIP ID such as @b 5100, @b 5200, @b 5500, and so on.
/**
* The set of critical section callback func.
*/
struct _CRIS
{
void (*_enter) (void); ///< crtical section enter
void (*_exit) (void); ///< critial section exit
}CRIS;
/**
* The set of @ref \_WIZCHIP_ select control callback func.
*/
struct _CS
{
void (*_select) (void); ///< @ref \_WIZCHIP_ selected
void (*_deselect)(void); ///< @ref \_WIZCHIP_ deselected
}CS;
/**
* The set of interface IO callback func.
*/
union _IF
{
/**
* For BUS interface IO
*/
//M20156501 : Modify the function name for integrating with W5300
//struct
//{
// uint8_t (*_read_byte) (uint32_t AddrSel);
// void (*_write_byte) (uint32_t AddrSel, uint8_t wb);
//}BUS;
struct
{
iodata_t (*_read_data) (uint32_t AddrSel);
void (*_write_data) (uint32_t AddrSel, iodata_t wb);
}BUS;
/**
* For SPI interface IO
*/
struct
{
uint8_t (*_read_byte) (void);
void (*_write_byte) (uint8_t wb);
void (*_read_burst) (uint8_t* pBuf, uint16_t len);
void (*_write_burst) (uint8_t* pBuf, uint16_t len);
}SPI;
// To be added
//
}IF;
}_WIZCHIP;
On the line " }CS;" I get the following errors:
#170 a function type is not allowed here
#18 expected a ")"
#80 expected a type specifier
Does anybody know how to resolve this problem?