Part Number: MSP432P401R
Hello Everyone,
I've been working on porting MSP-EXP432P401R LAUNCHXL to Zephyr RTOS. So far I'm able to get the zephyr binary generated and for programming the launchpad I have to use a command line utility which could program with .bin file.
I tried using Uniflash tool, but I'm getting the following error:
[ERROR] CS_DAP_0: Error connecting to the target: (Error -613 @ 0x0) The target indicates that it is busy. Either try the SWD request again, or abort the transaction. (Emulation package 6.0.628.3)
The above error is arising independent of the binary used. So, I suspect something wrong with the CMSIS-DAP interface.
But I can program the launchpad using CCS7.1.0 without any issues.
Any suggestions?