Part Number: MSP430F5528
Other Parts Discussed in Thread: LMT70, CC3100, LMT70EVM, CC2560, , CC3120MOD, CC2640R2F-Q1, CC3120, CC2640R2F, BOOST-CC2564MODA, MSP430F5529, CC31XXEMUBOOST
We have evaluated the LMT70 temperature transducer with the MSP430F5528 using the LMT70EVM and it works great for our application. We need a wireless connection and have both BT & WiFi connectivity options with our product uP controller. I'd like some guidance on the best option for our product and have been looking at the CC3100 and CC2560.
Our temperature measurement requirements are fairly basic. We will only have one device connected to our product uP controller at a time and all we want to do is periodically wakeup, read the LMT70 through the ADC of the MSP430F5228 (or similar), perform some calibration scaling and upload a temperature reading at a rate of 1-60 per min. We would also like to be able to download a new calibration lookup table occasionally if possible after performing a calibration process. Preferably the temperature probe with MSP430 and connectivity electronics could work at 120C.
We are looking for a minimum power consumption, simple, seamless, reliable connection solution. What would you recommend?