Other Parts Discussed in Thread: SIMPLICITI, CC2500, MSP430FG4618, TPS61097-33
Hey All,
I am working on a wireless application with the CC2500, MSP430 and Simpliciti. I Had a few questions.
What is a sound practice for unused pins on a layout? should I leave these floating, ground them, or use pull downs etc. Board size is a critical aspect of this project.
What are the bare minimum components requred to use an MSP430? (I amusing a msp430FG4168IPZ)
Anybody know a good battery (smaller the better) to use for such an application? Preferably one with a holder that will allow for easy swapping of batteries? I am using a TPS79933 (fixed 3.3V output) voltage regulator. I looked around and most of the "coin" style batteries had very very low max current outputs, on the order of 5-10mA even if they lasted for a long time.
Thanks
Paul