Part Number: MSP430FR5969
Tool/software: Code Composer Studio
Hello.
I was looking at MSP430FR5969 document (SLAS704E).
I could see that there are different operating mode exist in MSP430FR5969 device.
I have some things I was curious about.
1. what are the examples of High frequency peripherals and Low frequency peripherals
There is some example about 'Unclocked peripherals'but I could not find the information about 'high and low frequency peripherals'.
2. There is a section about Full retention.
I can see that only LPM3.5 and LPM4.5 is not supporting full retention.
Does it mean that I do not have to save CPU state, peripheral state, RAM contents, and register content to FRAM on LPM0~ LPM4?
Is it right that I have to save those features only on LPMx.5 mode?
------------------------------------------------------------------------------------------------
This questions are related with Question 1.
In section 6.3.1 Peripherals in LPM3 and LPM4,
I could see the information about peripheral groups
I would like to know if I understand correctly.
3. Is Group A available only in LPM3 and Is Group B available in both LPM3 and LPM4?
4. Are Group A and Group B distinguished by frequency?
Best,
Mirae