Part Number: MSP432P401R
Hi,
I am using msp432 internal ADC at 2.5V ref voltage with 14bit resolution. But with an input voltage of 1.6 V, I am getting 1.1V after conversion. There is a difference of 0.5 V. Even with a non RTOS code provided by TI, the value i get is 1.2 V for the same condition..
Please suggest how I can improve the accuracy of the reading? Also, How much tolerance should I consider for conversion results?
Thankyou,
- Suraj