Part Number: MSP430F67791A
Other Parts Discussed in Thread: LM5576
Dear All
I am currently designing a E-Meter which is powered by a 12V battery i have used the analog front end design as per the application note i have a few doubts here
1) I am powering the micro controller from a 12V car battery (since i need to operate a few high power relay based on the readings )
2) I am measuring the power of the a POLYPHASE
As per my design i have connected the neutral to AGND using a ferite bead, and for the digital gnd i am using the battery gnd. My point is since i am powering the micro controller with the battery + and - through an LM5576 LD0 , should i need to completely isolate the AVDD using a ferrite bead to isolate the DVDD(Output of LM5576 ) , or should i need to use any isolation transformers.