This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP-EXP430FR4133: Getting started with MSP-EXP430FR4133 and Energia

Part Number: MSP-EXP430FR4133
Other Parts Discussed in Thread: ENERGIA

Hello, I have just ordered a couple of MSP-EXP430FR4133 along with the accelerometer ADXL362, I have read conflicting threads and webpages about if i can use Energia to program the device. If not can i use Keil? Also I haven't been able to find any example code for this acclerometer / launchpad combo if anyone can find me an example or demo that would be much appreciated. 

  • Yes Chris, all MSP430 LaunchPads are supported by the Energia IDE. You should be able to find Energia accelerometer projects online that you can source from, the API has been designed such that it should be easy to port code between LaunchPad variants.

    Regards,
    Ryan

**Attention** This is a public forum