This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F5244: Program Crash during wait for stable clock at Init function.

Guru 24520 points

Part Number: MSP430F5244
Other Parts Discussed in Thread: MSP430F5242,

Hi TI Experts,

Please provide us your advice for my customer issue.

According to the customer, MSP430F5244 jumped to unexpected PC while waiting on stabled clock in part of init function when they used this mcu as 24MHz. But if they used the lower frequency for this device like 16MHz or 20MHz, this device worked. Also, they used the MSP430F5242 and ran the same program for this device, this phenomenon did not happen.

Have you ever seen this issue?
Would you please provide your advice in order to resolve this issue?

Best regards.
Kaka

**Attention** This is a public forum