Part Number: MSP430FR5739
Dear all,
After 50k pieces installed we got a strange behavior at the power ON of a MSP430FR5739
The application is a lighting control power through an 1-10 line that came from a AC.DC power supply, used as current generator for a string of LEDs.
The AC-DC could provide only a small amount of current, roughly 100-150uA, that produces a ramp on the capacitors on the PCBA.
From 0 to 10 V it takes roughly 1 seconds.
The microprocessor has a peak of current consumption at power ON. During the develop a lot of time was used to find a suitable order and settings in order to lower this peak.
In a lot of 2500 pieces it seems that, at the very beginning, when the voltage is increasing on the Vcc pins of the uP, the uP starts consuming too much letting the AC-DC find an equilibrium at roughly 1.6-1.8V. The uP, clearly it is not already started.
It seems that, once we found a “defective board”, if we move the microprocessor on one other board the defect follow the uP,
is connected to the power supply
Therefore:
1. Which are the starting currents when the MSP430FR5739 RHA 40pin is powered on?
2. Which variations of this parameter can we expect in production?
3. Are there known bugs that can lead to "abnormal" absorption
4. How can we conveniently set up the compiler?
5. Could you please support us in order to find an ideal order for the initial instructions to have the lowest possible peak power consumption at power ON?
6. Behavior "seems to be" highlighted with Lot BATCH NR components:
[)> 06P1PMSP430FR5739IRHAR6P2PJQ2500V00333171T4347111ZD74WTKYD163631T6793173CL620LDM621LUSA22LQAB23LPHLEG43Z3 / 260C / 168HR; //; 101616L15187K
7. The increase in consumption seems to follow the micro. An "abnormal" consumption card has returned to a common behavior after replacing the micro. The micro replaced replaces the abnormal consumption on the board where it was reinstalled.
8. How can coexist the 50000 pieces produced so far with the problems that we are now finding?
9. Electronic noise could bring the micro in the above described conditions.
10. How to connect the reset. Currently the PCBa have only a 49kOhm pull-up on reset, no capacitor to ground
11. Could you suggest a PMIC, low dropout able to produce the 2.04V to power the micro capable to resist up to 15V and with minimum quiescent current of few uA? It should also have a monitor circuitry able to enable it only once the input voltage it’s over 2.1V, possibly with an accurate monitor of the input voltage, to enable its output only for voltage voltages above 2.1Vdc
Best regards