Other Parts Discussed in Thread: MSP430USBDEVPACK
Hi,
I can run the numbers of max IO speed, SPI bus speed and theoretical USB Speed, but I was hoping someone could provide me with a max throughput speed I can expect with a 5528 doing nothing but moving data from USB to SPI. The customer wants to hit 5 mbit.
Full Speed USB should theoretically support 12mbit but with a 25mhz 430 clock, I was not sure we are even close to this theoretical...
This link above says worst case of approx 4mbit on the SPI. Can the 430 keep up moving data from the USB to the SPI at this throughput level - using DMA I assume?
Best Regards, Blake