This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP432P401R: strange verify flash error

Part Number: MSP432P401R
Other Parts Discussed in Thread: UNIFLASH

Hey,

I have build my own MSP432 hardware and it used to work great,

But now I have a strange problem with trying to debug the MSP432. When try to use CCS7.1 with the launchpad XDS110 debugger I have a failed to verify flash error. If I use uniflash to write a erase hex file don’t have any problems at all.  

 I tried to Upload the project directly to the MSP432 on the launchpad and that works just fine. So I think it has to be a hardware problem, but then the uniflash shouldn’t work either right?

I also already tried to factory reset the msp432 that dint help either.

The hardware setup I am using now is just a couple of decoupling capacitors and a header for the debug trace.

Greets,

Thijs

**Attention** This is a public forum