Part Number: MSP430FR5739
Other Parts Discussed in Thread: LPV521
Customer looking for more information beyond what is found in the User Guide
Specific questions:
- How to set the ADC clock if I want to use the device clock (not the MODOSC) which is set to 1MHz at the moment.
- How slow the ADC can go?
- The external VREF decoupling requirement is 10uF and 0.1uF – do you have any experience how critical is that value?
- What is the difference between the V(R+) = VEREF+ buffered and V(R-) = AVSS and the V(R+) = VEREF+ and V(R-) = AVSS?
- How much is the leaking on the input pin when it is in analog mode?
- What kind of LP filtering is recommended on the input pin? I’m driving it with a LPV521, so we need to consider what the LVP521 can drive.