This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR5869: ADC12_B

Guru 16770 points

Part Number: MSP430FR5869

Hi

Do you have answer to the following question?

1.

What is input impedance of ADC?

2.

Do you have information when input current sink leads to more or less impact for ADC?

Or is it no matter as long as input current is kept under the maximum of IveREF+/-?

BestRegards

**Attention** This is a public forum