Part Number: MSP430FR4133
Other Parts Discussed in Thread: MSP-FET
After developing an application using the MSP430FR4133, the first 16 devices where build
and testing has begun. One of these devices showed a correctable FRAM error. I've almost
forgotten the fact that I enabled the NMI for these errors over a year ago since I never
experienced them on my two test boards.
So i wonder if this single error seen here is the famous "it just happens once in a
lifetime but now it happened to you" error or it is something serious.
I didn't find a lot of real world statistics about FRAM errors -- just the note that
soldering the devices with an improper temperature could cause problems.
Yes, it was a correctable error and only one but I've no idea if I shoudl worry about it...