Other Parts Discussed in Thread: MSP-GANG,
Hi,
We are using MSP-GANG DLL for mass production.
As the current MSP-GANG was being for few years, we are trying to replace it with new programmers.
The MSP-GANG DLL doesn't work(cannot program) if use the older version of API firmware.
Error: "Failed ! Err 17 Header CRC"
Below are the details of the current MSP-GANG software.
Hardware G430: 01.02
Silicon Number 15D1 9046 1300 0100
API Firmware MSP-Gang A430: 01.01.10.00
BOOT Firmware G430BOOT B430: 01.00.02.00
GUI Software MSP-Gang-GUI G430: 01.01.10.00
DLL Software MSP-Gang-DLL D430: 01.01.10.00
Below are the details of the new MSP-GANG software.
Hardware G430: 01.04
Silicon Number 8A26 1147 2900 1300
API Firmware MSP-Gang A430: 01.01.10.00
BOOT Firmware G430BOOT B430: 01.00.02.00
GUI Software MSP-Gang-GUI G430: 01.01.10.00
DLL Software MSP-Gang-DLL D430: 01.01.10.00
We are trying to use the same software environment which we have used already.
But when we try to program the MSP's, it gives an error and we are not able to program.
Note: This problem occurs only when programming through DLL, it works fine when we
program directly through MSP-GANG (without DLL).
Note: Programming through DLL works if we update MSP-GANG API to version 01.02.04.00.
We have also tried to debug(step execute) the DLL through visual basic and all the functions
returns correct value during the first execution but the successive execution
goes wrong.
Please let us know if using 01.01.10.00 API Firmware on MSP-GANG version(01.04) is
not allowed, especially when programming through DLL?
If possible please let us know what could go wrong when programming through DLL and
the older version of API firmware.
Best Regards,