This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSPDRIVERLIB: CCS7.2 driverlib -- where do I put it?

Part Number: MSPDRIVERLIB

Tool/software: Code Composer Studio

I had to use the offline installer to get the ccs onto this computer.  And nothing shows up under Resource Explorer.  

I have manually downloaded the DriverLIB for the MSP432.  But I don't know where to put it.  Considering everyone else is havnig no difficulties in using it, I suspect there's something basic that I'm not seeing.  The code horks at the #include <ti/devices/msp432p4xx/driverlib/driverlib.h> line.  

This is getting very frustrating.  It used to be that you'd just install CCS and tada, you can start working.  Now there's a cloud and MSPWare (which I also don't seem to be able to get working) and such.  All I want is to be able to code for the MSP432 like I do the MSP430.  I clicked the boxes for the MSP432 -- why are none of the tools I need for that present?

**Attention** This is a public forum