Part Number: MSP430F67471
Hi everybody,
one of my customers has problem with the MSP430F67471 temperature sensor.
- It seems that the sensor is calibrated through TI at 30° and 85°. Thats correct right?
- The customer measured these temperatures and saw that these temp measurements are very good (+- 1k)
- But at negative temps they see that the error is about +- 5k. This error is way to high for them. They allow max +- 2k. Do we have a graph or something that shows the error at negative temps? Or can you explain why this high error occurs?
Now they want to understand why this error occurs and need more information about the sensor
- What is the principle of the temp sensor? PN with a diode? Transistor? or something else?
- Can the internal sensor measure negative temps? If yes what is the accuracy etc? Do we have app notes or TI-Designs reagrding the temp measurement with the MSP430F67471?
thank you
best regards
Bastian