Hello,
It seem that programming the microcontroller kill it. I'm using MSP-eZ430 programmer. Firstly I assembled an PCB and programed it succesfully. But when I ran debugger the board stopped working and i found that there is a direct short between 3.3V and gnd. Thinking that maybe I simply assembled it incorectly i tried another board(checking beforehand for any shorts) with the same result. When i investigated the circuit i found capacitor faulty capacitor. After replacing it i tried programming again with the same result (3.3 shorted to gnd). Thinking that maybe there is to much current coming out of the programmer i put some series resistance n the data and Vcc lines and but the result was the same. So finnaly i made a board with only the MSP430F2274 on it. After programming it i found the resistor heating up and the AVcc pin on the microcontroller blown.
I apreciate any advice.
Thank in advance