Part Number: MSP430F2002
Hi everybody ,
please I have a product with pcb working and in production using MSP430G2131IRSA16R .
now I need this product to be able to work up to 105 degrees celsius , keeping same pcb and ideally same sw .
for the micro I am moving to MSP430F2002TRSA so some questions :
1- as far as I see it should be a pin2pin drop in no issue at all : do you see anything special to consider ?
2- about SW do you have any indication / suggestion apart from changing headers ?
any suggestion is very welcome to speed up the process .
thank you
bye
Carlo