This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F5359: Launchpad

Part Number: MSP430F5359
Other Parts Discussed in Thread: MSP-EXP430F5529LP, MSP430F5529, MSP-FET

Hi,

I'm new to msp430 controller

We are planing to use msp430f5359, kindly suggest suitable launchpad that suits msp430f5359

Thank you

  • Hi!

    Unfortunately there is no LaunchPad with the MSP430F5359 assembled - there is one that has the MSP430F5529 on it: MSP-EXP430F5529LP. Maybe this is suitable for evaluating, too. There is also the generic MSP-TS430PZ100C that can be used with MSP430F5x and MSP430F6x 100 pin MCUs, so your selected one as well. But it requires a programmer like the MSP-FET, for example.

    Dennis

**Attention** This is a public forum