Part Number: MSP430FR6972
Tool/software: Starterware
Hi, sir
I set MCLK to 12MHz from DCO . From FRAM Part of msp430fr6972's user guide ,I knew "The system clock for the CPU or DMA can exceed the FRAM access and cycle time requirements. For these scenarios, a wait state generator mechanism is implemented. The Recommended Operating Conditions of the device-specific data sheet list the frequency ranges with the required wait state settings. " The Recommend Operating Conditions is following:
I confused the "NWAITSx" means. Do it represent the every bit of NWAITS[2:0], or not ? What should be set in NWAITS[2:0], if MCLK is 12MHz?
Another question , From msp430fr6072's device-specific data sheet ,the Supply Current is showed at different frequency of MCLK . I want to kow the speed of operation at different frequency of MCLK.
Cloud I understand that the speed of 16MHz MCLK is 16 times the speed of 1MHz MCLK ? So, 1MHz 's current consumption is assumed to be 210 uA, 16MHz‘s current consumption is assumed to be 1845 uA. Executing the same codes , 1MHz's time consumption is 16 times 16MHz. The 1MHz's current consumption is 210uA * 16 , and 16MHz's current consumption is 1845uA*1. Therefore, 1MHz's current consumption is large than 16MHz , when they execute same codes. Is it right ?
Best regards
Jent